SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Figure 3-1 CPSWSS Block DiagramThe CPSW subsystem provides Ethernet communication with hardware switching capabilities compliant to the IEEE 802.3 (Ethernet Working Group) standard. CPSW3G on AM26x devices supports 10Mbps, 100Mbps, or 1000Mbps operations with a selectable MII, RMII, or RGMII.
Port Architecture
SYSCFG automatically generates code and ENET-LLD handles the initial configuration. The application layer performs additional runtime configuration as necessary. Any packet entering the device externally enters through either the MAC port-1 or MAC port-2. If the packet is meant to be consumed by the device, the packet is forwarded to the host port. If the packet is meant to be sent to another port, the packet is switched to the other MAC port.
CPSW Sub-blocks
The CPSW subsystem is comprised of these smaller blocks:
Packet Classification
CPSW hardware can classify packets based on the following:
Based on the above list, a variety of rules can be set for consuming, forwarding, or dropping a packet on MAC ports. The CPSW also supports hardware-based modification of some of the above fields of the frame—offloading this operation from the CPU or software.
VLAN Support
Hardware VLAN tagging and filtering enables logical network segmentation. CPSW supports the following:
Use-cases include isolating the control plane from the traffic of the data plane, prioritizing safety-critical messages, and multi-tenant communication over shared physical infrastructure.
Rate Limiting
Policers enforce bandwidth limits at the ingress and egress of each MAC port. Packets that exceed the configured thresholds are dropped or remarked. Policers are essential for preventing congestion and maintaining fairness and deterministic latency in time-sensitive applications. Policers combined with QoS and VLAN tagging, provides complete traffic management for industrial Ethernet systems.