SLUUDO2 September   2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Acronyms
  5. 2Introduction
  6. 3Introduction to CPSWSS and ENET-LLD
    1. 3.1 Hardware
    2. 3.2 Software
    3. 3.3 Application Software
      1. 3.3.1 Board and Peripherals Initialization (SYSCFG)
      2. 3.3.2 CPSW Configuration (ENET-LLD)
      3. 3.3.3 Operating System (FreeRTOS or NoRTOS)
      4. 3.3.4 Middleware Stack (LwIP, Arm® Mbed™ Platform TLS, TSN)
      5. 3.3.5 Application Layer
  7. 4Debugging Hardware and Software
    1. 4.1 Hardware Debugging
      1. 4.1.1 Schematic Review Checklist
        1. 4.1.1.1 Management Data Input/Output (MDIO and MDC)
        2. 4.1.1.2 RGMII Interface
      2. 4.1.2 PHY Debug
        1. 4.1.2.1 PHY Bootstrap Settings
        2. 4.1.2.2 Trace Length
        3. 4.1.2.3 Clock Configuration
        4. 4.1.2.4 Mode Settings
        5. 4.1.2.5 IO MUX and SW Switch Settings
        6. 4.1.2.6 PHY Troubleshooting Guides
        7. 4.1.2.7 Custom Pin MUX Settings
      3. 4.1.3 Test Setup
      4. 4.1.4 Software Debugging
        1. 4.1.4.1 Using GEL Scripts in CCS
          1. 4.1.4.1.1 Statistics Using GEL Scripts
          2. 4.1.4.1.2 Statistics Using Expressions
      5. 4.1.5 Debugging Custom Ethernet Software
        1. 4.1.5.1 Debugging Initialization Sequence
        2. 4.1.5.2 PHY Debugging
        3. 4.1.5.3 MAC Port Debugging
        4. 4.1.5.4 TX Path Debugging
        5. 4.1.5.5 Systematic Debugging Checklist
          1. 4.1.5.5.1 RX Path Debugging
          2. 4.1.5.5.2 Multicast or Broadcast Does Not Work, But Unicast Works
    2. 4.2 Custom Hardware Bring-Up Process
      1. 4.2.1 Example 1: CPSW PHY Loopback
        1. 4.2.1.1 Failure: PHY Not Detected or MDIO Bus Not Alive
        2. 4.2.1.2 Failure: TX Packets Transmitted But RX Count = 0
      2. 4.2.2 Example 2: CPSW MAC Loopback Example
        1. 4.2.2.1 Failure: MAC Loopback Initialization Fails
        2. 4.2.2.2 Failure: TX Packets Increase But RX = 0
        3. 4.2.2.3 Failure: Nonzero Error Counters
      3. 4.2.3 Example 3: Enet_Layer2_CPSW and Enet_Layer2_cpsw_switch
        1. 4.2.3.1 Hardware Setup
        2. 4.2.3.2 Failure: Link Never Comes UP
        3. 4.2.3.3 Failure: Link is Up But No Frames Are Received or Transmitted
        4. 4.2.3.4 Failure: RX and TX Counters Increase But Error Rates Are High
      4. 4.2.4 Example 4: Enet_lwip_cpsw_example
        1. 4.2.4.1 Failure: Link Never Comes Up
        2. 4.2.4.2 Failure: Links Up But No IP Address Is Assigned
        3. 4.2.4.3 Failure: Ping Fails Despite Link and IP Address
    3. 4.3 Debugging Packet Forwarding Issues (ALE and Statistics)
      1. 4.3.1 CPSW Statistics Architecture
        1. 4.3.1.1 What Each Block Measures
        2. 4.3.1.2 Counter Reference Tables
          1. 4.3.1.2.1 MAC Port – RX Counters
          2. 4.3.1.2.2 MAC Port – TX Counters
          3. 4.3.1.2.3 MAC Port and Host Port – ALE and FIFO Drop Counters
          4. 4.3.1.2.4 Host Port – ALE Flood and Overrun Counters
          5. 4.3.1.2.5 MAC Port RX Issues
          6. 4.3.1.2.6 MAC Port TX Issues
          7. 4.3.1.2.7 Host Port RX Issues
          8. 4.3.1.2.8 Host Port TX Issues
    4. 4.4 Custom Board Enablement in SYSCFG
    5. 4.5 LwIP Debug Guide
      1. 4.5.1 LwIP Stack Configuration
      2. 4.5.2 lwip_stats
  8. 5Conclusion
  9. 6References
Host Port RX Issues

Frames arriving at the CPU DMA interface from the CPSW. rxGoodFrames here are meant to match macPort.rxGoodFrames minus any ALE drops. Any discrepancy is frames lost inside the switch on the path from the ALE to DMA.

Table 4-19 Host Port RX Statistical Summary
Scenario Nonzero Counter Root Cause Debug Method Fix | Reference
hostPort.rxGoodFrames is much less than macPort.rxGoodFrames; no ALE drops on the MAC port hostPort.rxBottomOfFifoDrop The DMA RX ring had no free entries. The application is not recycling buffers fast enough. Compare the wire RX rate versus the application packet counter. Check numRxPkts at initialization. Increase numRxPkts in the EnetDma_openRxFlow() function. Raise the RX task priority.
RX loss only under a sustained high rate hostPort.rxTopOfFifoDrop The DMA RX FIFO filled sustained back-pressure from slow processing. Monitor counter delta over 1s during burst. Increase the ring depth. Move RX processing to a higher-priority task.
The ALE drops visible in host port statistics hostPort.aleBlockDrop The state of the host port (port 0) ALE is not FORWARD. Issue CPSW_ALE_IOCTL_GET_PORT_STATE for port 0. Set port 0 to FORWARD: CPSW_ALE_IOCTL_SET_PORT_STATE.
The ALE drops at the host port; tagged traffic hostPort.aleVidIngressDrop The VLAN on the incoming frame is not registered for the host port in the ALE. Dump the ALE table – check the VLAN entry includes port 0. Add or update the VLAN entry with the host port in the member list.
The CPU is starved by broadcast or multicast hostPort.aleUnknownBcast or aleUnknownMcast very high Storm traffic flooded to host port; no ALE rate limiter Check counter delta over 1s; compare the Host Port Rx Counter with the normal traffic baseline. Configure the rate limiter: CPSW_ALE_IOCTL_SET_PORT_BCAST_MCAST_LIMIT.
Policer drops are accumulating hostPort.aleRateLimitDrop The policer of the ALE is active – the rate limit is potentially too aggressive. Verify the configured rate limit value. Check if the traffic is legitimate. Increase the limit or register multicast groups explicitly with CPSW_ALE_IOCTL_ADD_MCAST.