SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The PHY loopback example tests the internal loopback mode of the external chip of the PHY. The test enables the loopback register (typically bit 14 of the PHY control register) of the PHY to route transmitted packets directly back to the receiver within the PHY silicon.
Location: source/networking/enet/core/examples/enet_loopback/enet_cpsw_loopback/
The example tests the path from the CPU to the PHY and back.
Figure 4-15 CPSW PHY Loopback FlowSuccessful demonstration of the PHY loopback on the custom board means that the path to and from the CPU to the PHY is correct. If the examples fail, then there is some issue with one or more of the components. The following sections provide some sample failure cases.