SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Hardware statistics counters provide the fastest path to isolating packet forwarding failures on the CPSW. For pinpointing the root cause, the CPSW STATS can be leveraged to find where the issues lie, whether in the ALE, MAC port, or host port configurations. STATS is a functional block in CPSW.
There are two ways to get the statistical values:
The key principle is that the statistics counter signature reveals the failure mode.
Table 4-12 lists some of the common issues that can be uncovered using CPSW statistics.
| Issue Symptom | Primary Counters to Examine |
|---|---|
| The frame counts look correct but data is corrupted | rxCrcErrors, rxAlignCodeErrors, and rxOversizedFrames |
| Intermittent RX loss under high load | rxBottomOfFifoDrop, rxTopOfFifoDrop, and aleOverrunDrop |
| The application sends Ethernet packets but nothing appears on the wire | portMaskDrop, txSofOverrun, and MAC txGoodFrames |
| Packets arrive at the wire but the application receives nothing | portMaskDrop, aleDrop, and rxBottomOfFifoDrop |
| Traffic tagged as VLAN silently drops | aleVidIngressDrop and aleBlockDrop |
| Broadcast and multicast storm—throughput degrades | aleRateLimitDrop, aleUnknownBcast, and aleUnknownMcast |