SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The link negotiation succeeded, but the packet is not received or transmitted.
| Cause | How to Check | Fix |
|---|---|---|
| The ALE port is not in the FORWARD state | Check the ALE port state (is meant to be FORWARD not LEARN/DISABLED). | Verify the ALE is configured to forward frames. |
| MAC RX is not enabled | Check if the EnetDma_openRxFlow() function succeeded. | Verify the DMA RX channel configuration in code. |
| The RX buffer pool is empty | Check rxFreeQ has buffers before test. | Increase LargePoolPktCount in SYSCFG. |
| The TX descriptors are not configured | Check if the EnetDma_openTxCh() function succeeded. | Verify the TX DMA channel is open. |
| The MAC address is not in the ALE | The frame potentially drops if the ALE did not learn the frame. | Send the broadcast frame to trigger ALE learning. |
| The frame size exceeds MTU | The RX controller potentially drops oversized frames. | Check that the frame is ≤ 1500 bytes (or configured as MTU). |