SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Both MAC port statistics and host port statistics contain the same ALE and FIFO drop fields. When present in MAC port statistics, the fields describe drops of frames ingressing from MAC port n; when present in host port statistics, the fields describe drops of frames ingressing from the CPU DMA path.
| Counter | Struct Field | Root Cause |
|---|---|---|
| ALE generic drop | aleDrop | Sum of all ALE policy drops (the below mentioned counters start from ALE overrun drops) |
| ALE overrun drop | aleOverrunDrop | ALE lookup FIFO overran – sustained burst exceeded ALE capacity |
| Port mask drop | portMaskDrop | ALE lookup resolved the DA but the result portmask excluded the destination port |
| RX bottom-of-FIFO drop | rxBottomOfFifoDrop | Ingress FIFO empty when frame arrived – immediate DMA starvation |
| RX top-of-FIFO drop | rxTopOfFifoDrop | Ingress FIFO full when frame arrived – sustained DMA back-pressure |
| ALE rate limit drop | aleRateLimitDrop | ALE policer classified frame as exceeding configured rate limit |
| ALE VID ingress drop | aleVidIngressDrop | VLAN ID of incoming frame not registered on the ingress port |
| ALE DA=SA drop | aleDAEqSADrop | Destination address equals source address – loopback detection |
| ALE block drop | aleBlockDrop | Ingress port state is BLOCKED – most common new-port misconfiguration |
| ALE secure drop | aleSecureDrop | SA of incoming frame bound to a different port in a secure VLAN |
| ALE auth drop | aleAuthDrop | Port requires 802.1x authentication; port is not yet authorized |