SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The Layer 2 CPSW example is a simple Ethernet forwarding application that receives frames from an external network, processes these frames in the application, and forwards the frames back. The example tests the complete real-world data path with link negotiation, frame reception, and transmission.
Location: source/networking/enet/core/examples/enet_layer2_cpsw/, source/networking/enet/core/examples/enet_layer2_cpsw_switch/
This test is the first real network test. If this test fails, the problem is in the PHY configuration, external connectivity, and ALE. The example helps to test the following factors: