SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The board prints an IP address ping <board-ip> from the PC and gets no reply.
| Cause | How to Check | Fix |
|---|---|---|
| The ALE is not forwarding unicast to the host port | macStats.rxGoodFrames > 0 but hostStats.rxGoodFrames = 0; check macStats.portMaskDrop. | Verify the ALE host port is in the FORWARD state. Check that the DA entry portmask includes bit 0. |
| There is DMA RX buffer starvation | hostStats.rxBottomOfFifoDrop > 0. | Increase numRxPkts in the EnetDma_openRxFlow() function using SYSCFG. |
| LwIP NETIF is not set to UP | netif_is_up(&netif) returns false in debugger. | Verify that the netif_set_up() function is called after the netif_add() function completes in the main_loop() function. |
| The ARP request dropped | macStats.rxGoodFrames = 0 on the ARP of the PC. There is no response from the board. | Check hostStats.aleUnknownUcast; confirm the broadcast ALE entry is present. |
| The PC and board are on different subnets | The IP addresses differ in subnet (for example, 192.168.1.x versus 10.0.0.x). | Assign the PC IP to same /24 subnet as the board; check the gateway settings. |
Furthermore, if other stacks are used, for example the LLDP, gPTP, MbedTLS, and so forth, the specific examples can be tested.