SLLSFE8B November 2024 – November 2025 TCAN2845-Q1 , TCAN2847-Q1
PRODUCTION DATA
The device has two thermal sensors in the device to monitor the junction temperature of the die.
There is a thermal shutdown pre-warning provided that is set when the junction temperature of VCC1 LDO,and external PNP control, VEXCC, hits the warning temperature level. When this temperature sensor reaches the pre-warning rising, TSDWR, an interrupt is set for pre-warning. There are three interrupts a thermal event. The behavior of the device depends upon which sensor hits the thermal event. This is a device preservation feature.
Exceeding the maximum junction temperature for > tTSD causes interrupt flags to be set and is indicated by pulling nINT low. If VCC1 or VEXCC causes the TSD event; the device turns off these LDOs and enter either fail-safe mode (if enabled) or sleep mode. The nRST pin is pulled to ground during this TSD event. Once the over temperature fault condition has been removed and the junction temperature has cooled beyond the TSDF temperature for 1s, the device transitions from fail-safe mode to restart mode and turn on VCC1 and VEXCC (if enabled). A thermal shut down interrupt flag is set but not indicated on nINT pin as VCC1 is off. This event turns off the high side switches by resetting the HSS1-4_CNTL registers. If thermal shutdown event happens while the device is in fail-safe or sleep mode and cyclic sensing is enabled, the cyclic sensing function is lost as HSS4 is turned off.
If TSD is detected by the second sensor which covers the transceivers and VCC2. Both CAN and LIN transmitters is disabled placing them into listen mode. VCC2 LDO is disabled and the interrupt flag is set. This does not cause an SBC state change. Once the over temperature fault condition has been removed and the junction temperature has cooled beyond the TSDF temperature, the CAN and LIN transmitters is re-enabled. After 1s of further wait time, VCC2 LDO is turned on. Note that UVCC2 is not set because the LDO has been disabled. Read VCC2_STATUS at register 8'h4F[2] to determine when VCC2 has been re-enabled. If VCC2 is used in the system as the supply source for VCAN, then the VCC2 off condition creates a UVCAN condition. The CAN transceiver changes to wake capable, and cannot be re-enabled until VCC2 is fully powered again. VCC2_STATUS is also indicating the status of VCAN. When VCC2_STATUS=1b, the CAN transceiver is re-enabled and UVCAN interrupt flag can be cleared.