SLLSFE8B November 2024 – November 2025 TCAN2845-Q1 , TCAN2847-Q1
PRODUCTION DATA
Registers 8’h13, 8'h14, and 8’h16 configure the watchdog function. The TCAN284x-Q1 watchdog can be set as a timeout, window, or Q&A watchdog by setting 8’h13[6] to the method of choice. The timer, tWD, for each of these watchdog configurations is based upon registers 8’h13[5:4] WD prescaler and 8’h14[7:5] WD timer and is in ms. See Table 8-16 for the achievable times and more detail. If using smaller time windows, use the timeout version of the watchdog, but not required. This is for times between 4ms and 64ms. The programmed time is also used for the Q&A watchdog which is programmed at registers 8'h2D through 8'h2F where 8'h2D is the configuration register.
| WD_TIMER | 8'h13[5:4] WD_PRE | |||
|---|---|---|---|---|
| 8'h14[7:5] | 00 (default) | 01 | 10 | 11 |
| 000 | 4 | 8 | 12 | 16 |
| 001 | 32 | 64 | 96 | 128 |
| 010 | 128 | 256 | 384 | 512 |
| 011 (default) | 256 | 384 | 512 | 768 |
| 100 | 512 | 1024 | 1536 | 2048 |
| 101 | 2048 | 4096 | 6144 | 8192 |
| 110 | 10240 | 20240 | RSVD | RSVD |
| 111 | RSVD | RSVD | RSVD | RSVD |
The watchdog timing can only be configured in standby mode if unlocked.