SWRU626 December 2025 CC3501E , CC3551E
Each GPTIMER has the same number of outputs as channels, but each channel does not control a dedicated output. Instead every channel can control every output. Which output each channel controls is configured in the CnCFG.OUTn fields.
The user can set and clear timer outputs manually by writing OUTCTL. Manual update of an output takes priority over automatic channel updates of the same output. Listed in decreasing order of priority, each output can:
An output can receive update requests from several channels at the same time. In this case, the output is updated according to the priority list. The output updated from an channel is decided by the channel action, CnCFG.CCACT.