SWRU626 December 2025 CC3501E , CC3551E
DSP is a single-phase format where WCLK is high for one BCLK period, and the MSB of the first sample word is typically aligned with this WCLK pulse, or it follows in the next BCLK period. Sample words for subsequent audio channels are then transferred back-to-back, followed by an idle period until the next phase or frame begins. Data is sampled on the falling edge of BCLK and updated on the rising edge of BCLK. The below figure shows the DSP serial format with zero data delay.
Figure 22-5 DSP Serial Format