SWRU626 December 2025 CC3501E , CC3551E
The purpose of the activation flow is to perform a one-time action per device by the vendor to switch the device ownership from TI to the vendor to secure its IP. This means that from this point on, any vendor IP stored on the device cannot be accessed by anyone without vendor privileges and credentials.
The CC35xx device executes the boot sequence for device activation in two stages through a Chain of Trust that terminates at TI level.
A detailed description of the flow is as follows:
If successful, from this point on – the device is associated with the vendor who owns the private key whose hash of public key is installed on the device.
This ROT installation and identification method is a common industry good security practice and part of the MCUboot infrastructure.