SWRU626 December 2025 CC3501E , CC3551E
Table 3-75 lists the memory-mapped registers for the DCB registers. All register offset addresses not listed in Table 3-75 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Section |
|---|---|---|---|
| 10h | DHCSR | Controls halting debug | Section 3.9.3.1 |
| 14h | DCRSR | With the DCRDR, provides debug access to the general-purpose registers, special-purpose registers, and the FP extension registers. A write to the DCRSR specifies the register to transfer, whether the transfer is a read or write, and starts the transfer | Section 3.9.3.2 |
| 18h | DCRDR | With the DCRSR, provides debug access to the general-purpose registers, special-purpose registers, and the FP Extension registers. If the Main Extension is implemented, it can also be used for message passing between an external debugger and a debug agent running on the PE | Section 3.9.3.3 |
| 1Ch | DEMCR | Manages vector catch behavior and DebugMonitor handling when debugging | Section 3.9.3.4 |
| 24h | DAUTHCTRL | This register allows the external authentication interface to be overridden from software. | Section 3.9.3.5 |
| 28h | DSCSR | Provides control and status information for Secure debug | Section 3.9.3.6 |
Complex bit access types are encoded to fit into small table cells. Table 3-76 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
DHCSR is shown in Table 3-77.
Return to the Summary Table.
Controls halting debug
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-27 | RES0 | R | 0h | Reserved, RES0 |
| 26 | S_RESTART_ST | R | 0h | Indicates the PE has processed a request to clear DHCSR.C_HALT to 0. That is, either a write to DHCSR that clears DHCSR.C_HALT from 1 to 0, or an External Restart Request |
| 25 | S_RESET_ST | R | 0h | Indicates whether the PE has been reset since the last read of the DHCSR |
| 24 | S_RETIRE_ST | R | 0h | Set to 1 every time the PE retires one of more instructions |
| 23-21 | RES0_1 | R | 0h | Reserved, RES0 |
| 20 | S_SDE | R | 0h | Indicates whether Secure invasive debug is allowed |
| 19 | S_LOCKUP | R | 0h | Indicates whether the PE is in Lockup state |
| 18 | S_SLEEP | R | 0h | Indicates whether the PE is sleeping |
| 17 | S_HALT | R | 0h | Indicates whether the PE is in Debug state |
| 31-16 | DBGKEY | W | 0h | A debugger must write 0xA05F to this field to enable write access to the remaining bits, otherwise the PE ignores the write access |
| 16 | S_REGRDY | R | 0h | Handshake flag to transfers through the DCRDR |
| 15-6 | RES0_2 | R | 0h | Reserved, RES0 |
| 5 | C_SNAPSTALL | R/W | 0h | Allow imprecise entry to Debug state |
| 4 | RES0_3 | R | 0h | Reserved, RES0 |
| 3 | C_MASKINTS | R/W | 0h | When debug is enabled, the debugger can write to this bit to mask PendSV, SysTick and external configurable interrupts |
| 2 | C_STEP | R/W | 0h | Enable single instruction step |
| 1 | C_HALT | R/W | 0h | PE enter Debug state halt request |
| 0 | C_DEBUGEN | R/W | 0h | Enable Halting debug |
DCRSR is shown in Table 3-78.
Return to the Summary Table.
With the DCRDR, provides debug access to the general-purpose registers, special-purpose registers, and the FP extension registers. A write to the DCRSR specifies the register to transfer, whether the transfer is a read or write, and starts the transfer
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-17 | RES0 | R | 0h | Reserved, RES0 |
| 16 | REGWnR | W | 0h | Specifies the access type for the transfer |
| 15-7 | RES0_1 | R | 0h | Reserved, RES0 |
| 6-0 | REGSEL | W | 0h | Specifies the general-purpose register, special-purpose register, or FP register to transfer |
DCRDR is shown in Table 3-79.
Return to the Summary Table.
With the DCRSR, provides debug access to the general-purpose registers, special-purpose registers, and the FP Extension registers. If the Main Extension is implemented, it can also be used for message passing between an external debugger and a debug agent running on the PE
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBGTMP | R/W | 0h | Provides debug access for reading and writing the general-purpose registers, special-purpose registers, and Floating-point Extension registers |
DEMCR is shown in Table 3-80.
Return to the Summary Table.
Manages vector catch behavior and DebugMonitor handling when debugging
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-25 | RES0 | R | 0h | Reserved, RES0 |
| 24 | TRCENA | R/W | 0h | Global enable for all DWT and ITM features |
| 23-21 | RES0_1 | R | 0h | Reserved, RES0 |
| 20 | SDME | R | 0h | Indicates whether the DebugMonitor targets the Secure or the Non-secure state and whether debug events are allowed in Secure state |
| 19 | MON_REQ | R/W | 0h | DebugMonitor semaphore bit |
| 18 | MON_STEP | R/W | 0h | Enable DebugMonitor stepping |
| 17 | MON_PEND | R/W | 0h | Sets or clears the pending state of the DebugMonitor exception |
| 16 | MON_EN | R/W | 0h | Enable the DebugMonitor exception |
| 15-12 | RES0_2 | R | 0h | Reserved, RES0 |
| 11 | VC_SFERR | R/W | 0h | SecureFault exception halting debug vector catch enable |
| 10 | VC_HARDERR | R/W | 0h | HardFault exception halting debug vector catch enable |
| 9 | VC_INTERR | R/W | 0h | Enable halting debug vector catch for faults during exception entry and return |
| 8 | VC_BUSERR | R/W | 0h | BusFault exception halting debug vector catch enable |
| 7 | VC_STATERR | R/W | 0h | Enable halting debug trap on a UsageFault exception caused by a state information error, for example an Undefined Instruction exception |
| 6 | VC_CHKERR | R/W | 0h | Enable halting debug trap on a UsageFault exception caused by a checking error, for example an alignment check error |
| 5 | VC_NOCPERR | R/W | 0h | Enable halting debug trap on a UsageFault caused by an access to a coprocessor |
| 4 | VC_MMERR | R/W | 0h | Enable halting debug trap on a MemManage exception |
| 3-1 | RES0_3 | R | 0h | Reserved, RES0 |
| 0 | VC_CORERESET | R/W | 0h | Enable Reset Vector Catch. This causes a warm reset to halt a running system |
DAUTHCTRL is shown in Table 3-81.
Return to the Summary Table.
This register allows the external authentication interface to be overridden from software.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
| 3 | INTSPNIDEN | R/W | 0h | Internal Secure non-invasive debug enable. Overrides the external Secure non-invasive debug authentication interface |
| 2 | SPNIDENSEL | R/W | 0h | Secure non-invasive debug enable select. Selects between DAUTHCTRL and the external authentication interface for control of Secure non-invasive debug |
| 1 | INTSPIDEN | R/W | 0h | Internal Secure invasive debug enable. Overrides the external Secure invasive debug authentication Interfaces. |
| 0 | SPIDENSEL | R/W | 0h | Secure invasive debug enable select. Selects between DAUTHCTRL and the external authentication interface for control of Secure invasive debug. |
DSCSR is shown in Table 3-82.
Return to the Summary Table.
Provides control and status information for Secure debug
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-18 | RES0 | R | 0h | Reserved, RES0 |
| 17 | CDSKEY | R/W | 0h | Writes to the CDS bit are ignored unless CDSKEY is concurrently written to zero |
| 16 | CDS | R/W | 0h | This field indicates the current Security state of the processor |
| 15-2 | RES0_1 | R | 0h | Reserved, RES0 |
| 1 | SBRSEL | R/W | 0h | If SBRSELEN is 1 this bit selects whether the Non-secure or the Secure version of the memory-mapped Banked registers are accessible to the debugger |
| 0 | SBRSELEN | R/W | 0h | Controls whether the SBRSEL field or the current Security state of the processor selects which version of the memory-mapped Banked registers are accessed to the debugger |