Descriptions of exception handling use
the following terms.
- Preemption: An exception can preempt the current execution if its
priority is higher than the current execution priority. When one exception
preempts another, the exceptions are called nested exceptions.
- Return: This occurs when the exception handler is completed. The
processor pops the stack and restores the processor state to the state it had
before the interrupt occurred.
- Tail-Chaining: This mechanism speeds up exception servicing. On
completion of an exception handler or during the return operation, if there is a
pending exception that meets the requirements for exception entry, then the
stack pop is skipped and control transfers directly to the new exception
handler.
- Late Arriving Interrupts: This mechanism speeds up preemption. If a
higher priority exception occurs during state saving for a previous exception,
the processor switches to handle the higher priority exception and initiates the
vector fetch for that exception. State saving may be affected by the late
arrival depending on the stacking requirements of the original exception and the
late-arriving exception. On return from the exception handler of the
late-arriving exception, the normal tail-chaining rules apply.