SWRU626 December 2025 CC3501E , CC3551E
This channel action continuously:
The channel generates center-aligned PWM waveform when CTL.MODE = UPDWN_PER. The channel copies a new value written in PCnCC to CnCC when CNTR becomes 0. This action prevents jitter on the edges of the generated PWM signal. Similarly, the timer copies a new value written in PTGT to TGT when CNTR becomes 0. This action avoids period-jitter in PWM applications with time-varying periods.
Example: Center-Aligned PWM Generation by Channel 0
This example illustrates center-aligned PWM generation by channel 0. The waveform is synthesized on output 0. The timer period is kept static, and the target value is set to half the period. Configure as follows:
The duty-cycle of the generated PWM waveform is controlled by PC0CC updates. Waveform generation on event output 0 continues until aborted by the user.
If the user wants to stop/pause the PWM generation in a controlled manner, the following procedure is recommended: