SLUSFQ1A December 2024 – December 2024 BQ41Z90
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
The BQ41Z90 AFE has the ability to blow an external fuse in the event of a permanent failure. The fuse drive itself is supplied from the BAT input pinand its state can be monitored using the AIF_ANA_DIN register. To drive the FUSE output set AIF_CTRL2 [FUSE_BLOWD] = 1. When the firmware is not intending to drive the FUSE pin then the fuse drive can be configured to monitor for activity on the FUSE pin from an external source such as a second level voltage protector.
If the FUSE output is not used, it should be connected to VSS. When FUSE is in the low state, it uses an internal weak pullup to detect disconnection between the FUSE pin and the fuse drive circuitry.