SBASAO8 June 2025 DAC39RF20
ADVANCE INFORMATION
When a frame alignment character (/F/) or multi-frame alignment character (/A/) is detected in an unexpected location, LANE_ERR[7] is set. No monitoring is performed for missing alignment characters.
The frame alignment monitor inspects both /F/ and /A/ characters to determine if they aligned to the frame boundary. If two characters (either two /F/, two /A/, or one of each) are received in an unexpected location with respect to the frame boundary without receiving an alignment character at an expected frame boundary location, LANE_ERR[5] is set and SYNC is asserted to restart the link.
The multi-frame alignment monitor inspects only /A/ characters to determine if they are aligned to the multi-frame boundary. If two multi-frame alignment characters are received at an unexpected location with respect to the multi-frame boundary without receiving a multi-frame alignment character at an expected multi-frame boundary location, LANE_ERR[6] is set and SYNC is asserted to restart the link.
If the transmitter sends 4 successive /K/ characters after the start of the ILAS, both LANE_ERR[5] and LANE_ERR[6] is set and SYNC is asserted to restart the link.
Frame and multiframe alignment correction is not supported. Two consecutive frame or multiframe alignment errors causes the link to restart.