SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
The PWM_EN bit, when set enables the DPWM channel. If it is 0 (default), the DPWM outputs are set to the value in the DPWM Fault Polarity bits (Section 2.15.10).
Note that if edge generation is enabled, the bits will be controlled by the edge gen logic. To make the bits go to the desired values, it will be necessary to clear the EDGE_EN bit in DPWMEDGEGEN.
This bit occurs only in the Control 0 register, not in the AMS registers.