SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
Several 3138 family members have multiple flash blocks. This doesn’t change the basic programming code, but it increases flexibility. It is not necessary to execute from RAM or Data Flash when erasing or writing to program flash. It can also be done while executing from any other flash block than the one being changed. It is not possible to write or erase two blocks at the same time however.