SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
In the past, the filter was called a Control Law Accelerator, so for historical reasons, the Filter Enable bit is called CLA_EN. This bit, when set, causes the DPWM to take its input from a Filter. Otherwise, the DPWM output comes from the DPWM registers only.
This bit is duplicated in the AMS registers.
The filter which controls each DPWM is selected by the DPWMx_FILTER_SEL bit in the DPWMMUX register in the Loop Mux.