SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
All members of UCD3138 family of Controllers share the same core functions and features. But each one of these devices also offers some unique abilities that may not exist in the other members of the family. The following table is arranged in order to direct you to the right manual for a specific device of your interest.
A downloading link is provided at the intersection only if the specific manual is needed for certain device.
| Device\Manual | Migration Guide, Device Enhancement Summary |
|---|---|
| UCD3138 | |
| UCD3138A | SLUA741 |
| UCD3138064 | SLUUAD8 |
| UCD3138064A | SLUA766 |
| UCD3138A64 | SLUUB54 |
| UCD3138128 | SLUUB54 |
| UCD3138128A | SNIU030 |
The description of modules and peripherals in UCD3138 family of controllers is explained in this manual and complimentary migration manuals.
The simplest configuration of the Digital Power Peripherals highlighting the key blocks involved in loop control is shown below:
Figure 1-1 The Error ADC (in the Front End) accepts a differential voltage signal as an input. It measures the difference between this input and a digitally controlled reference voltage and generates a digital error output. It passes this digital error information to the Filter. The Error ADC (or EADC) is a specialized high speed, high resolution ADC with a small dynamic range, optimized for power supply error measurement.
The Filter takes the error signal and passes it through a PID based digital filter which compensates for the characteristics of the external loop. This filter can be dynamically reprogrammed for changing power load source, and circuit characteristics. It also offers non-linear response capability for better handling of transients.
The output of the compensator is passed to a Digital PWM (DPWM) generator. The DPWM has two outputs, which can be used in many different ways. There are modes for synchronous rectification, multiple phases, various bridge topologies, and LLC configurations. In addition to the 2 DPWM outputs, the DPWM has other signals which are used externally and internally. These include:
These signals will be covered in much more detail in Chapter 2.
The peripherals can be run tied together as shown above, or they can be used in different groupings and interconnections, not shown in the picture above. For example, the DPWM can be used to trigger the Error ADC, which will trigger the Filter at the end of its conversion.
The UCD3138 device supports multiple sets of the Digital Power Peripherals affording the ability to control upto 3 feedback loops (voltage or current) and drive 8 outputs simultaneously. To inter-connect all the DPPs, there is a large module called the Loop Mux. This permits a high degree of flexibility in DPP configuration. Any Front End can be connected to any Filter, and any Filter output can be connected to any DPWM. Additionally, information can be passed between the peripherals. For example, the output of one Filter (eg. controlling a slow Voltage loop), can contribute to the reference of another Front End (eg. monitoring a fast current loop) and enable implementation of nested loops (such as in Average Current mode control).
In addition, the DPPs in UCD3138 provide other modules and functions for power supply and control. These include:
There is also a module called Fault Mux which connects fault detection circuitry outputs to control inputs, primarily on the DPWMs, to customize fault handling and recovery.
This documentation provides information about the DPP modules in UCD3138, starting with a detailed description, continuing with some configuration examples, and ending with a reference section which lists each bit field in each DPP module.