SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
The MIN_DUTY_MODE bits select how the DPWM handles minimum duty cycle limits.
There are two registers setting minimum duty and hysteresis:
DPWMMINDUTYLOW
DPWMMINDUTYHI
The Low register sets the point at which the minimum duty mode will take effect as the duty drops. In mode 2, it also sets the minimum duty.
The High register sets the point at which minimum duty mode is exited as the duty goes up.
These bits are not duplicated in the AMS registers.
These two graphs show modes 1 and 2 with PMMINDUTYLOW at 30, and DPWMMINDUTYHI at 70.
Figure 2-15 Minimum Duty Mode 1
Figure 2-16 Minimum Duty Mode 2