SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
If the MAN_SLAVE_ACK bit is set, then the firmware must manually ACK the slave address. Normally this is used if there are multiple addresses which must be decoded, and where the mask register will not cover them all. Here is the sequence when a write occurs:
Figure 10-8 Slave Address Manual ACK for WriteThe steps are:
The manual slave ACK has no effect on later bytes in the sequence, so there is no need to show full sequences with manual slave ACK at the beginning. All sequences will be the same as if there is an automatic slave ACK after step 4 in the figure above.