SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
The OUTPUT_MULT_SEL bits select what value is multiplied by the filter output to determine the DPWM pulse width. See the Section 5.14.6 for specific bit assignments. The options are:
Note that the default is KComp. This is not intuitive, especially for users of the UCD3000 series digital power controller. They UCD3000 had no options in this area, period was always used. It is easy to overlook this bitfield when setting up for a simple period based system. The OUTPUT_MULT_SEL register works with the FILTERMUX register in the Loop Mux for value selections. FILTERMUX selects which KComp is used, which DPWM Period is used, and which Filter output is used for Feed Forward. Resonant Duty also comes from a DPWM module and is also selected by FILTERMUX. See 5.4 Filter Mux Register (FILTERMUX).
Switching Period is provided by the DPWM. The default is the value from the DPWM Period register, and this is used for most topologies. However, there are two other DPWM registers which can also be sent to the Filter for this value. See 2.17.3 Filter Duty Select, for more details.