SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The recommendation is to connect USB0_ID pin directly to the corresponding ID pin on a USB Micro-AB connector. Depending on the cable attached, the USB0_ID pin is terminated and the processor can be configured as host or device.
Full compliant USB On-The-Go (OTG) feature is not supported.