SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The recommendation is to connect the ADC0 analog supply VDDA_ADC0 to the recommended power supply rails in the processor-specific data sheet.
The recommendation is to follow the notes added at the end of the Signal Descriptions, ADC, MAIN Domain table of the processor-specific data sheet before using ADC0.
Refer section Peripherals, Analog-to-Digital Converter (ADC), Change Summary of AM64x / AM243x SR2.0 ADC Errata of Hardware Design Considerations for Custom Board Design Using AM6442, AM6422, AM6412 and AM2434, AM2432, AM2431 (ALV, ALX) Processor Families user's guide.
ADC0 inputs are not fail-safe. Applying a voltage to any of the ADC0 inputs before powering the processor is not recommended or allowed. The input applied (based on the input level) can cause residual voltage on the processor supply rail and can result in board start-up issues. Refer Absolute Maximum Rating table of processor-specific data sheet. In case supply rails that are available before the processor supply ramps are required to be monitored, the recommendation is to connected these inputs to the ADC0 through a switch. The switch can be controlled by processor GPIO or power good signal from any of the supply source including PMIC.