SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The below FAQ includes recommendations on CAP_VDDSn capacitor value, and the effect of the capacitor assembly (mounted or shorted):
The processor families support x7 (seven) dual-voltage IO supply for IO groups (VDDSHVx [x = 0-5]) and IO supply for IO group MCU (VDDSHV_MCU). Each IO supply for IO group is connected (referenced) to a fixed set of IOs. Each IO supply for IO group can be connected to fixed (VDDSHV5 supports dynamic supply switching) 3.3V or 1.8V supply independently. The IO supply for IO group defines a common operating voltage for the entire set (fixed set) of IOs.
Processor pads (pins) designated as CAP_VDDSn [n = 0-5] and CAP_VDDS_MCU connects the external capacitor to the internal IO supply for IO group regulator when the IO supply for IO groups connect to 3.3V supply (optional when IO supply for IO groups supplies connect to 1.8V). A 1μF (connected between the pins and VSS, see the processor-specific data sheet) capacitor is recommended. See the processor-specific data sheet for the recommended capacitor voltage rating and allowed capacitance range. When IO supply for IO groups are connected to 3.3V, the steady state DC output VDDSHVx/2, is the voltage to be considered for choosing the capacitor voltage rating considering the DC bias effect.
A 3.3μF (recommended tolerance is ± 20%) capacitor is recommended to be connected between the pin CAP_VDDSHV_MMC1 and VSS.
To minimize PCB loop inductance, place the capacitors on the back side of the PCB in the array of the BGA. The choice of capacitor voltage rating influences capacitor package (size) selection.
The recommendation is to select capacitor with ESR < 1Ω, keep the trace loop inductance < 2.5nH.
A number of processor IOs are not fail-safe. For information on available fail-safe IOs, see the processor-specific data sheet. The recommendation is to connect the IO supply of attached devices to the same power source connected to the respective processor dual-voltage IO supply for IO group (VDDSHVx) to make sure the custom board design never applies potential to any of the processor IOs that is not powered. Applying external input to the IOs that are not fail-safe when IO supply for IO groups supply is not available can affect the processor functionality, performance and reliability.
For more information on power-sequencing requirements between the processor and attached devices including signal isolation for fail-safe operation, see the following FAQ:
The FAQ is generic and can also be used for AM64x and AM243x processor families.
The recommendation is to verify that a valid supply voltage for the VDDSHVx is present before applying input to the associated processor IOs or peripherals.
The recommendation is to connect the VDDSHVx supplies and associated CAP_VDDSn (when IO supply connected is 3.3V, optional for 1.8V) capacitor irrespective of the usage of the processor IOs or peripherals.