SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The Voltage and Thermal Manager (VTM) module on the processor supports voltage and thermal management of the processor by providing control of on-chip temperature sensors.
Independent temperature sensors are located at designated hotspots on the processor. The recommendation is to read the on-die temperature sensors in Linux and perform thermal management. See the E2E thread.
The processor supports one VTM module, VTM0, which is located in the MAIN domain.
For more information, see the following FAQ: