General
Review and verify the
following for the custom schematic design:
- Reviewed above
"Common checklist for all
sections" section of the user's guide.
- Configuration of
processor clock input source, crystal + internal oscillator
or external oscillator.
- Selection of
crystal, crystal frequency and crystal load capacitor.
- Selection of
MCU_OSC0 external crystal load capacitor.
- Connection
recommendations when crystal + internal oscillator or
external oscillator is used.
- Connection of XO
when external oscillator output is connected to XI.
Schematic
Review
Follow the below list for
the custom schematic design:
- Connection of 25MHz MCU_OSC0 clock is
mandatory.
- Selection
of External crystal or External clock oscillator as
per the data sheet requirements.
- Verify
the crystal, crystal frequency and crystal load
capacitor selected follows processor-specific data
sheet recommendations.
- 25MHz is
the clock input frequency currently supported. Refer
processor-specific data sheet for supported clock
input frequencies.
- Direct
connection of crystal (without series or parallel
resistor) and connection of the crystal load
capacitance circuit (MCU_OSC0) as per
processor-specific data sheet.
- External
crystal load capacitor is recommended to be x2 of
the crystal load, including PCB capacitance
(~4pF).
- The
recommendation is to select crystal load value such
that a standard value capacitor can be selected for
the load capacitor.
- The
recommendation is to retain the HFOSC0 registers in
the default state.
- When
external oscillator is used, the recommendation is
to add decoupling capacitor and a bulk capacitor
near to the oscillator supply pin and series
resistor on the clock output pin.
- The
recommendation is to connect XO to VSS when external
oscillator (LVCMOS clock) output is connected to
XI.
- Addition
of series resistor (22Ω) on the clock output pin
close to the oscillator.
Additional
- Refer to the
Applications, Implementation, and Layout
section of the processor-specific data sheet for clock
routing guidelines.
- The
recommendation is to connect the 25MHz (performance has been
validated only with 25MHz frequency) crystal directly to the
processor XI and XO pins, no series or parallel resistors
are recommended. The internal oscillator implements
Automatic Gain Control (AGC) for amplitude control.
- Processor-specific data sheet shows that MCU_OSC0 does not
start until the core voltage ramps because there are some
cases where the oscillator does not start until VDD_CORE
ramps. In most of the use cases, the oscillator starts when
VDDS_OSC supply ramps (although the oscillator starting when
VDDS_OSC ramps is not always the case). The oscillator
start-up diagram in the processor-specific data sheet shows
the maximum start-up time, which includes the case where the
delay is based on VDD_CORE being valid.
- A DC steady-state
condition is not allowed on MCU_OSC0_XI because MCU_OSC0_XI
is internally AC coupled to a comparator that can enter an
unknown state.
- The LVCMOS clock
sourcing the MCU_OSC0_XI input is required to have monotonic
transitions and shall be connected to MCU_OSC0_XI with a
point-to-point connection, via a series resistor placed near
the clock source. The series termination resistor value
shall match the clock source output impedance to the
transmission line impedance. For example, a 20Ω is used when
clock source has 30Ω output impedance and the PCB signal
trace has 50Ω characteristic impedance. This allows the
reflection that returns from the far end of the unterminated
transmission line to be completely absorbed to not introduce
any non-monotonic events.
- The
recommendation is to minimize the PCB trace length
connecting the external clock source to MCU_OSC0_XI. This
reduces capacitive loading and minimizes probability of
external noise sources coupling to the clock signal. Reduced
capacitive loading improves rise/fall times of the clock
signal which reduces the probability of jitter being
introduced (to the clock source or the custom board).
- The
recommendation is to verify the crystal selection with the
crystal supplies or manufacturer.