SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The recommendation is to connect USB0_DM and USB0_DP signals directly from the processor to the USB hub upstream port. The hub then distributes USB0 signals to the downstream ports. Ground the connector ID to enable host mode. As each hub has different implementation requirements, the recommendation is to follow the hub manufacturer recommendations.
For more information on USB2.0 interface, see the following FAQs: