SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
During the design phase of custom board design, in case any discrepancy is seen between the processor-specific EVM or SK and processor-specific data sheet during processor evaluation or custom board design, the recommendation is to follow the processor-specific data sheet. Despite the best efforts by the EVM or SK designer, the EVM or SK schematic can have errors that still function but are not completely aligned with the processor-specific data sheet specifications.