SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: clb_ex30_cyclic_redundancy_check.c
For the detailed description of this example, please refer to: C2000Ware_PATH\utilities\clb_tool\clb_syscfg\doc\CLB Tool Users Guide.pdf
In this example, the CLB module is used to perform the cyclic redundancy check (C.R.C.) with twelve messages in bits checked with ten different CRC polynomials.
First element passed in is message length, second is the message stored in input_data
This example is only available for CLB types 2 and up.
The known values in the output_data are compared with expected values from the CLB-based CRC calculation. A total of 120 messages are verified, and the number of matching messages are displayed in passCount
Variables to add to Watch Expressions in debug view: passCount - number of messages that match between generated and known CRC values failCount - number of messages that fail the CRC value verification