SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The receive ready (RXRDY) flag is set when the SCI transfers newly received data from SCIRXSHF to SCIRD. The RXRDY flag therefore indicates that the SCI has new data to be read. Receive interrupts are enabled by the SET RX INT bit. If the SET RX INT is set when the SCI sets the RXRDY flag, then a receive interrupt is generated. The received data can be read in the Interrupt Service routine.
On a device with both SCI and a DMA controller, SET RX DMA must be cleared to select interrupt functionality.