SPRUJ42E March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
PRODUCTION DATA
Transmit event and error clear register.
Return to Summary Table
| Instance Name | Physical Address |
|---|---|
| FSI_TX0 | 5028 002Ch |
| FSI_TX1 | 5028 102Ch |
| FSI_TX2 | 502A 002Ch |
| FSI_TX3 | 502A 102Ch |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED_1 | |||||||
| R | |||||||
| 0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED_1 | PING_TRIGGERED | BUF_OVERRUN | BUF_UNDERRUN | FRAME_DONE | |||
| R | W | W | W | W | |||
| 0h | 0h | 0h | 0h | 0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15:4 | RESERVED_1 | R | 0h | Reserved |
| 3 | PING_TRIGGERED | W | 0h | Ping Frame Triggered Flag Clear bit This bit clears the corresponding bit in the TX_EVT_STS register. 0h[W] = Writing a 0 to this bit will have no effect. 1h[W] = Writing a 1 to this bit will clear the corresponding bit in the TX_EVT_STS register to 0. Note: This bit may not always be cleared when Writing to the corresponding TX_EVT_CLR bit. If PING_TIMEOUT MODE is configured to be 0, a hardware ping timeout may occur when another frame is actively being transmitted. In this case, if this bit still shows as 1 after the clear bit is written then the ping frame has been triggered but not serviced. This bit does not indicate that the ping frame has been completely sent, only that it has been triggered by the timeout event. |
| 2 | BUF_OVERRUN | W | 0h | Buffer Overrun Flag Clear bit This bit clears the corresponding bit in the TX_EVT_STS register. 0h[W] = Writing a 0 to this bit will have no effect. 1h[W] = Writing a 1 to this bit will clear the corresponding bit in the TX_EVT_STS register to 0. |
| 1 | BUF_UNDERRUN | W | 0h | Buffer Underrun Flag Clear bit This bit clears the corresponding bit in the TX_EVT_STS register. 0h[W] = Writing a 0 to this bit will have no effect. 1h[W] = Writing a 1 to this bit will clear the corresponding bit in the TX_EVT_STS register to 0. |
| 0 | FRAME_DONE | W | 0h | Frame Done Flag Clear bit This bit clears the corresponding bit in the TX_EVT_STS register. 0h[W] = Writing a 0 to this bit will have no effect. 1h[W] = Writing a 1 to this bit will clear the corresponding bit in the TX_EVT_STS register to 0. |