JAJSKX2A August 2019 – May 2021 TPS53676
PRODUCTION DATA
Use MFR_CALIBRATION_CONFIG command to adjust the gain and offset of the input current sensor. First, set analog front-end gain such to keep the signal at the ADC to be less than 800 mV. Then set the digital gain to fine-tune the total gain based on the selected input current shunt. Finally adjust the input current offset based on lab measurements. A detailed example of input current sensor calibration is shown in Pin Functions. .
The equation for input current sense measurements is shown in Equation 8.
where
Estimate the maximum input current for the design using Equation 9.
where
Select the analog front-end gain, GIINSHUNT, to maximize the signal level at the ADC whie remaining within its full scale range of 800 mV. Select the closest available value less than the result of Equation 10.
Finally select the digital gain factor, GIINMAX, with a resolution of 0.5 per LSB, to fine-tune the current sense gain using Equation 11.
Example: 12V to 1.0 V 4+0 design at 100 A, RSENSE = 1.0 mΩ
Channel B is not used in this design. Estimate the maximum input current, according to the calculation below.
Select the analog front-end gain, and digital gain factors as shown below. Set the IIN_OFS to 0.0 A, and tune based on design characterization measurements.
Finally, the calibrated input current measurement is verified to be calibrated properly.