JAJSFD3G August   2016  – March 2019 DRA786
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
Sysboot

NOTE

For more information, see the Initialization (ROM Code) section of the Device TRM.

Table 4-24 Sysboot Signal Descriptions

SIGNAL NAME DESCRIPTION TYPE BALL
sysboot0 Boot Mode Configuration 0. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I E8
sysboot1 Boot Mode Configuration 1. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I A7
sysboot2 Boot Mode Configuration 2. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I F8
sysboot3 Boot Mode Configuration 3. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I B7
sysboot4 Boot Mode Configuration 4. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I A6
sysboot5 Boot Mode Configuration 5. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I F7
sysboot6 Boot Mode Configuration 6. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I E7
sysboot7 Boot Mode Configuration 7. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I R7
sysboot8 Boot Mode Configuration 8. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I B6
sysboot9 Boot Mode Configuration 9. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I A5
sysboot10 Boot Mode Configuration 10. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I D6
sysboot11 Boot Mode Configuration 11. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I C5
sysboot12 Boot Mode Configuration 12. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I B5
sysboot13 Boot Mode Configuration 13. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I D7
sysboot14 Boot Mode Configuration 14. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I B4
sysboot15 Boot Mode Configuration 15. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. I A4