SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
This section defines basic sequence flow chart divided into several sub sequences.
UHSII is not supported. For more information, see Not Supported Features.
"Wait for interrupts" is used in the flow chart. This means the Host Driver waits until specified interrupts are asserted. If already asserted, then fall through that step in the flow chart. Timeout checking shall be always required to detect no interrupt generated but this is not described in the flow chart.
This specification uses the double box like Figure 12-212, (the step (1) in Figure 12-216), it means that the other flows, which already are shown, shall be performed. Therefore, the interrupt may be included in the other flows.
Figure 12-212 Double Box Notation