SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Figure 7-27 illustrates the counter-compare submodule within the EPWM. Figure 12-311 shows the basic structure of the counter-compare submodule.
Figure 12-310 EPWM Counter-Compare SubmoduleCC module features:
The counter-compare submodule takes as input the time-base counter value. This value is continuously compared to the counter-compare A (EPWM_CMPA) and counter-compare B (EPWM_CMPB) registers. When the time-base counter is equal to one of the compare registers, the counter-compare unit generates an appropriate event.