Trace distribution is accomplished
using standard Arm®
CoreSight™ compliant trace infrastructure components:
- CoreSight™ Trace Funnels (CSTF): Non-programmable
CSTFs are used at points of interleaving where multiple trace sources
converge and form a single stream of trace traffic. This device includes one
instance of a programmable CSTF that is deployed immediately before the
TPIU.
- CoreSight™ Trace Replicator (CSREP): A
programmable CSREP is used as a routing device, that can be used to forward
trace traffic, based on its ID, to one, both, or none of the device trace
sinks.