SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The CSI_RX_IF will default to stop processing the frame whenever a header Reserved DT or ECC error is detected, or when a long packet payload CRC is identified.
The CSI_RX_IF will detect the error condition and capture the associated VC, DT and WC information for the packet header before generating an error interrupt flag on CSIRX_ERROR_IRQS.
The CSI_RX_IF will stop processing the current frame and stop the stream.
Figure 12-413 Stream Error Detection Causing Stop