SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Booting from an eMMC device is only available on Port 0 of the MMCSD controller (MMCSD0). Booting from an eMMC device is not available on Port1 (MMCSD1)
The ROM will boot from eMMC devices using one of these methods:
To boot from UDA in either raw or filesystem mode, choose bootmode "MMCSD Boot" (see Table 5-4).
A special alternate boot mode is available with eMMC devices which allows the ROM to boot from an image that is in a separate boot partition in the eMMC. To boot from this mode, choose "eMMC Boot" (see Table 5-4).
The ROM Code will start reading from the memory boot sector, or filesystem, as specified by the BOOTMODE pin (FS/Raw). Only FAT32 and FAT16 formats are supported in filesystem mode. It will continue reading data from the memory and storing it in internal RAM until a complete image has been read. In RAW mode, the ROM supports a redundant image at offset 0x400000 in case the initial image fails to be recognized. When the complete image has been read and found in good integrity, the ROM Code will branch to the address defined in the Boot Info field of the boot header.
When eMMC boot is used as a backup boot option, only User Data Area (UDA) in filesystem mode is supported. Raw mode is not supported. Additionally, boot will only occur in 1-bit mode during backup booting.