SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Events mapped to the low priority error interrupt (ESM_INT_LOW_LVL_0) are intended to be events of interest that should be addressed eventually, not events that require immediate attention. An example would be an event indicating a corrected error. The system may want to track this for statistical purposes, but it does not require immediate attention.
Any error event can be mapped to the low priority error interrupt. A low priority error interrupt will be generated when an event is enabled to cause an interrupt (via the ESM_INTR_EN_SET_j register) and mapped to the low priority error interrupt (via ESM_INT_PRIO_j register) and the raw status is set (via the ESM_RAW_j register).
When a low priority error interrupt is received, the acting processor must perform the following steps:
The global event map is neither defined by nor maintain in ESM. The global event map must be defined and maintained by software using software determined memory resources. It is conceivable that the global event map will be predefined and loaded during the execution of a secondary boot loader.
The rest of the steps assume that the error has been handled and the system wants to clear the error event. Clearing the error event depends on whether the event is a level (see Section 12.8.2.4.1.2.1) or pulse (see Section 12.8.2.4.1.2.2) event.