SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Table 10-1 lists the interrupts that are generated by the GICSS.
| Interrupt Name | Description |
|---|---|
| GICSS0_AXIM_ERR_0 | GICSS bus error interrupt. This interrupt is triggered if the GICSS receives an error on a bus transaction, such as a decode or protection error. This is a pulse-high interrupt. If this interrupt occurs, the GICSS might lose interrupts and must be reset. If it is not reset, behavior becomes unpredictable. |
| GICSS0_ECC_FATAL_0 | GICSS uncorrectable ECC error interrupt. Indicates an uncorrectable 2-bit error detected in one of the ITS cache memories. This is a pulse-high interrupt. If this interrupt occurs, the GICSS might lose interrupts and must be reset. If it is not reset, behavior becomes unpredictable. |
| GICSS0_ECC_AGGR_CORR_LEVEL_0 | GICSS ECC aggregator correctable (SEC) error interrupt |
| GICSS0_ECC_AGGR_UNCORR_LEVEL_0 | GICSS ECC aggregator uncorrectable (DED) error interrupt |
| GICSS0_GIC_PWR0_WAKE_REQUEST_0 | GICSS wake requests for A53 cores. Asserted state indicates that an interrupt is pending for a processor that has set the PROCESSORSLEEP bit in the GICR_WAKER register. This bit indicates that the SoC should wake up the indicated CPU so that it can process the interrupt. |
| GICSS0_GIC_PWR0_WAKE_REQUEST_1 |