SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Because this device muxes GPIO signals with other functional signals, the availability of any particular GPIO and hence the usability of its associated interrupt will change based on the use case pin muxing. The large number of possible GPIO interrupt sources makes it impractical to route all interrupt events to each processing element. Since most applications do not typically require a large number of GPIO interrupts, the interrupt uncertainty is resolved by mapping all GPIO interrupts to a series of event muxes implemented using Interrupt Router (IntRouter) modules. These muxes allow any one of the available GPIO interrupts to be selected and passed on as an event to the various processor interrupt controllers and DMA controllers. Event selection is controlled through associated registers within each IntRouter.
The GPIO bank interrupts already represent a consolidation of the 16 GPIO interrupts associated with each bank and are routed directly to various interrupt controllers rather than through the GPIO IntRouters.
One of the GPIO pins has a potential use case as an Arm reset input and should therefore be routed as highest priority interrupt in the GIC and mapped to nFIQ in software.
Figure 12-4 shows the GPIO Interrupt Routers connectivity. Refer to Interrupt Routers, for more details on the GPIO Interrupt Routers connectivity.