SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
After POR and device initialization occurs, the hardware loads the stack pointer from flash or ROM based on the presence of an application in flash and the state of the EN bit in the BOOTCFG register. If the flash address 0x0000.0004 contains an erased word (value 0xFFFF.FFFF) or the EN bit is of the BOOTCFG register is clear, the stack pointer and reset vector pointer are loaded from ROM at address 0x0100.0000 and 0x0100.0004, respectively. The bootloader executes and configures the available boot slave interfaces and waits for an external memory to load its software. The bootloader uses a simple packet interface to provide synchronous communication with the device. The speed of the bootloader is determined by the internal oscillator (PIOSC) frequency. The following serial interfaces can be used:
If the check of the flash at address 0x0000.0004 contains a valid reset vector value and the EN bit in the BOOTCFG register is set, the stack pointer and reset vector values are fetched from the beginning of flash. This application stack pointer and reset vector are loaded and the processor executes the application directly. Otherwise, the stack pointer and reset vector values are fetched from the beginning of ROM.
Figure 7-2 shows the bootloader selection sequence.
Figure 7-2 Boot Configuration Flow