SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
The timers each have a dedicated µDMA channel and can provide a request signal to the µDMA controller. Pulse requests are generated by a timer via its own dma_req signal. A dma_done signal is provided from the µDMA to each timer to indicate transfer completion and trigger a µDMA done interrupt (DMAnRIS) in the GPTM Raw Interrupt Status Register (GPTMRIS) register. The request is a burst type and occurs whenever a timer raw interrupt condition occurs. The arbitration size of the µDMA transfer should be set to the amount of data that should be transferred whenever a timer event occurs.
For example, to transfer 256 items, 8 items at a time every 10 ms, configure a timer to generate a periodic time-out at 10 ms. Configure the µDMA transfer for a total of 256 items, with a burst size of 8 items. Each time the timer times out, the µDMA controller transfers 8 items, until all 256 items have been transferred. See Section 8 for more details about programming the µDMA controller.
A GPTM DMA Event (GPTMDMAEV) register is provided to enable the types of events that can cause a dma_req signal assertion by the timer module. Application software can enable a dma_req trigger for a match, capture or time-out event for each timer using the GPTMDMAEV register. For an individual timer, all active timer trigger events that have been enabled through the GPTMDMAEV register are ORed together to create a single dma_req pulse that is sent to the µDMA. When the µDMA transfer has completed, a dma_done signal is sent to the timer resulting in a DMAnRIS bit set in the GPTMRIS register.