SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
The UART can generate interrupts when the following conditions are observed:
All of the interrupt events are ORed together before being sent to the interrupt controller, so the UART can only generate a single interrupt request to the controller at any given time. Software can service multiple interrupt events in a single interrupt service routine by reading the UART Masked Interrupt Status (UARTMIS) register (see Section 26.5.12).
The interrupt events that can trigger a controller-level interrupt are defined in the UART Interrupt Mask (UARTIM) register (see Section 26.5.10) by setting the corresponding IM bits. If interrupts are not used, the raw interrupt status is visible via the UART Raw Interrupt Status (UARTRIS) register (see Section 26.5.11).
NOTE
For receive time-out, the RTIM bit in the UARTIM register must be set to see the RTMIS and RTRIS status in the UARTMIS and UARTRIS registers.
Interrupts are always cleared (for the UARTMIS and UARTRIS registers) by writing a 1 to the corresponding bit in the UART Interrupt Clear (UARTICR) register (seeSection 26.5.13).
The receive time-out interrupt is asserted when the receive FIFO is not empty, and no further data is received over a 32-bit period when the HSE bit is clear or over a 64-bit period when the HSE bit is set. The receive time-out interrupt is cleared either when the FIFO becomes empty through reading all the data (or by reading the holding register), or when a 1 is written to the corresponding bit in the UARTICR register.
The receive interrupt changes state when one of the following events occurs:
The transmit interrupt changes state when one of the following events occurs: