| 15 |
RESERVED |
R |
0x0 |
|
| 14 |
PRBSM |
R/W |
0x0 |
PRBS Single/Continuous Mode.
0x0 = Single mode selected. When BIST Error Counter reaches its max value, the PRBS checker stops counting.
0x1 = Continuous mode selected. When the PRBS counters reach maximum count value, the counter starts counting from zero again.
|
| 13 |
PRBSPKT |
R/W |
0x0 |
Generated PRBS Packets.
0x0 = When packet generator is enabled, generate a single packet with constant data. PRBS generation and check is disabled.
0x1 = When packet generator is enabled, generate continuous packets with PRBS data. When packet generator is disabled, PRBS checker is still enabled.
|
| 12 |
PKTEN |
R/W |
0x0 |
Packet Generation Enable.
0x0 = Disable packet generator
0x1 = Enable packet generation with PRBS data
|
| 11 |
PRBSCHKLK |
R |
0x0 |
PRBS Checker Lock Indication.
0x0 = PRBS checker is not locked
0x1 = PRBS checker is locked and synchronized on received bit stream
|
| 10 |
PRBSCHKSYNC |
R |
0x0 |
PRBS Checker Lock Sync Loss Indication.
0x0 = PRBS checker has not lost synchronization.
0x1 = PRBS checker has lost synchronization on received bit stream. This is an error indication.
|
| 9 |
PKTGENSTAT |
R |
0x0 |
Packet Generator Status Indication.
0x0 = Packet Generator is disabled.
0x1 = Packet Generator is active and generate packets.
|
| 8 |
PWRMODE |
R |
0x1 |
Power Mode Indication.
0x0 = Indicates that the PHY is in one of the sleep modes, either active or passive.
0x1 = Indicates that the PHY is in normal power mode.
|
| 7 |
RESERVED |
R |
0x0 |
|
| 6 |
TXMIILB |
R |
0x0 |
Transmit Data in MII Loopback Mode.
0x0 = Data is not transmitted to the line in MII loopback
0x1 = Enable transmission of the data from the MAC received on the TX pins to the line in parallel to the MII loopback to RX pins. This bit may be set only in MII Loopback mode, which is enabled by setting the MIILOOPBK bit in the EPHYBMCR register, offset EPHY.0x00.
|
| 5 |
RESERVED |
R |
0x0 |
|
| 4-0 |
LBMODE |
R/W |
0x0 |
Loopback Mode Select. The PHY provides several options for Loopback that test and verify various functional blocks within the PHY.
0x00 = Reserved
0x0 = Reserved
0x01 = Near-end loopback: PCS Input Loopback
0x02 = Near-end loopback: PCS Output Loopback (In 100Base-TX only)
0x03 = Reserved
0x04 = Near-end loopback: Digital Loopback
0x05 = Reserved
0x6 = Reserved
0x7 = Reserved
0x08 = Near-end loopback: Analog Loopback (requires 100-Ω termination)
0x09 = Reserved
0xA = Reserved
0xB = Reserved
0xC = Reserved
0xD = Reserved
0xE = Reserved
0xF = Reserved
0x10 = Far-end Loopback: Reverse Loopback
|