SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Figure 15-79 shows an asynchronous multiple-read operation on a nonmultiplexed device in which two word32 host read accesses to the GPMC are split into one multiple- (page mode of 4 word16) read access to the attached device.
Figure 15-79 Asynchronous Multiple (Page Mode) ReadThe WAIT signal is active low.
The nCS, nADV, nOE, and DIR signals are controlled in the same way as address/data-multiplexed accesses (see Table 15-447).
When RDACCESSTIME completes, control signal timings are frozen during the multiple data transactions, corresponding to PAGEBURSTACCESSTIME multiplied by the number of remaining data transactions.
Read data is latched at GPMC_CONFIG5_i[20:16] RDACCESSTIME completion time (where i = 0 to 7). The end of the access is defined by the GPMC_CONFIG5_i[4:0] RDCYCLETIME parameter.
During consecutive accesses, the GPMC increments the address after each data read completes.
Delay between successive read data in the page is controlled by the GPMC_CONFIG5_i[27:24] PAGEBURSTACCESSTIME parameter. Depending on the device page length, the GPMC can control device page crossing during a burst request and insert initial RDACCESSTIME latency. Page crossing is possible only with a new burst access, meaning a new initial access phase is initiated.
Total access time RDCYCLETIME corresponds to RDACCESSTIME, plus the address hold time, starting from the nCS deassertion.